UNIVERSAL ROBOTS WITH ATI’S F/T SENSORS JUST FEEL RIGHT
Six-Axis Force/Torque (F/T) sensors from ATI deliver the highest accuracy, precision, and reliability in a compact and durable package. F/T sensors are comprised of a rugged transducer body that is mounted between the robot flange and end-of-arm tooling. The latest addition to ATI’s F/T product family is the Axia80. This new, high-performance, low-cost offering maintains the high quality and accuracy found in all ATI F/T products. The Axia80 is compatible with all UR robot models and is available as a complete sensing package through the UR+ online showroom.
Read More >
|
|
|
ACIETA AND ATI MAKE METAL FABRICATING EASIER
Automation integrator, Acieta, has developed a new system that enables medium- to high-volume metal fabricators to reduce costs and offset labor shortages. The Robotically Integrated Bending Solution (RIBS), employs robotic automation for press brake machine tending. A robotic arm outfitted with ATI Tool Changers presents parts to the brake and provides a method for changing the press brake tooling automatically. Acieta and ATI are helping customers increase the productivity and flexibility of their press brakes and reduce safety concerns associated with manual machine tending.
Read More >
|
|
|
PRE-TEC INTEGRATES ATI TOOL CHANGERS IN A FAST FINISHING SOLUTION
The Robotic Cardboard Applicator System from PRE-TEC offers Oriented Strand Board (OSB) manufacturers a way to protect their products during transit and helps keep inventory costs low. PRE-TEC developed an innovative set up for this application; Tool Changers from ATI increase productivity, but keep the system’s footprint small. PRE-TEC’s system is convenient for manufacturers. It provides a one-step, value-added, finishing process that helps to ensure the OSB arrives at its final destination in perfect condition. ATI’s Tool Changers are integral in providing flexibility to this application.
Read More >
|
|
|
ATI’S F/T SENSORS GIVE KINDHEART SURGICAL SIMULATORS "ALL THE FEELS"
Surgeons and surgical teams are known for their ability to perform with accuracy under immense pressure. Timing and efficiency are critical to the success of many procedures, but practicing first is not always an option. With KindHeart surgical simulators, surgical teams can learn to perform at even higher levels, while gaining insight into what a patient experiences during the process. With the help of ATI’s Force/Torque (F/T) sensors, KindHeart’s surgical simulation devices are able to capture feedback from forces exerted on a patient during surgery.
Read More >
|
|
|
ATLAS COPCO DESIGNS A FASTENING SYSTEM FOR A FLEXIBLE FUTURE
Atlas Copco’s PF6 Flexsystem, the company’s latest fixtured tightening system, is designed with the future in mind. Using ATI’s Heavy-Duty Robotic Tool Changers, Atlas Copco is able to achieve a modular work cell that leaves plenty of manufacturing floor space and flexibility for today’s ever-changing automotive assembly environment. For Atlas Copco, adaptable and flexible production lines are integral to their customer’s productivity. ATI’s Tool Changers and Tool Stands play a vital role in delivering that capability. The PF6 Flexsystem handles multiple tasks while reducing cycle time and overall footprint.
Read More >
|
|
|
|
Featured Products
AXIALLY-COMPLIANT FINISHING TOOL MODEL ACT-390
These finishing tools are robust, low-speed, high-torque air tools with an axially floating spindle, suitable for a multitude of robotic and non-robotic material finishing operations of aluminum, plastic, steel, and more.
Read More >
|
MANUAL TOOL CHANGER FOR COLLABORATIVE APPLICATIONS
The MC-10 Manual Tool Changer provides a cost-effective solution for quickly changing tools by hand and is optimized for collaborative robot applications.
Read More >
|
|
Featured Videos
UNIVERSAL COMPLIANCE COMPENSATOR (UCC) DEMONSTRATES BIN-PICKING
The Universal Compliance Compensator (UCC) complies in many directions and allows the robot to overcome severe misalignment between the tool and workpiece.
View >
|
RADIALLY-COMPLIANT DEBURRING TOOLS USED FOR AUTOMATED WHEEL DEBURRING
iA-ROBOTICS has developed an automated wheel-deburring system that utilizes ATI's Radially-Compliant Deburring Tools. The system increases quality of finished goods and reduces scrap.
View >
|
|
ATI exhibits at a variety of industry shows and conferences. Our schedule is listed below. Contact Valerie Van Deusen
here
if you would like a ticket or pass (subject to availability) to any upcoming shows.
IMTS 2024
|
September 9-14, 2024
|
McCormick Place | Chicago, IL (Booth #236144)
|
|
Fabtech 2024
|
October 15-17, 2024
|
Orange County Conv. Center | Orlando, FL (Booth #5281)
|
|
|